Technical FAQs

Ask a Question

Is Channel level diagnostic possible for 140DDI35300 and 140DDO35300 IO module.

There is no channel level diagnostic available for 140DDI35300 and 140DDO35300 but yes we can read the health status of complete module by using syetem word from %SW180 to %SW339. Address can be selected as per the module position.
Refer Unity pro Help for detail.
Was this helpful?
What can we do to improve the information ?