Technical FAQs

Ask a Question

What is the correspondence between the wire colours of cable VW3A8306D30 and the pin numbers of the RJ45 socket?

The correspondence between the wire colours of cable VW3A8306D30 and the pin numbers of the RJ45 socket is as follows:


Was this helpful?
What can we do to improve the information ?