Technical FAQs

Ask a Question

How to connect Pressure Sensor XMLK006B2C21 on ATV303 drive.

Analog output of pressure sensor XMLK006B2C21 is 4 to 20mA.
 
Program 204.0 [AI1 type] to 0A [Current: x-y mA] in AI1 CONFIGURATION MENU
Program 204.1[AI1 current scaling parameter of 0%] to 4mA in AI1 CONFIGURATION MENU
Program 204.2[AI1 current scaling parameter of 100%] to 20mA in AI1 CONFIGURATION MENU
 
Connect 4 to 20mA analog output from Pressure Sensor to Analog Input of ATV303 (AI1 and COM).
And program 512.2[High speed] to 50 Hz.
 
Scaling=> 4mA corresponds to 0 Hz and 20mA corresponds to 50 Hz.
 
So, when pressure sensor Analog output is 20mA, then Drive will run at 50 Hz.

 
Was this helpful?
What can we do to improve the information ?