Technical FAQs

Ask a Question

What is the material composition for push button XB7NA31 and XB7NA42.

Material composition for XB7NA31 and XB7NA42 (same ratios for both):
- Polyamide                      : 72%
- Steel                              : 16%
- Butylen polyterephtalate  :  9%
- Elastomere                     :  2%
- Brass                             :  0.5%
 
Was this helpful?
What can we do to improve the information ?