Technical FAQs

Ask a Question

What is the material of Limit switch body ZCMD61 contacts.

Limit switch body ZCMD61 contacts are silver contacts covered with 3 micron gold.
 
Was this helpful?
What can we do to improve the information ?