Technical FAQs

Ask a Question

Why in Ecodial software the discrimination between Compact NSX100B (micrologic) with Acti9 iC60N/H 63A is showing as Total Discrimination where as in Complemetary Technical guide shows the partial discrimination limit upto 6kA for the same.

If the fault current at the switchboard is <6 kA, Ecodial is showing "TOTAL discrimination"  This is because the Ik3 Max < 6kA

where as if the fault current is just above 6 kA, in this case, there is a discrimination limit of 6 kA.

Complementary Technical Guide :

Was this helpful?
What can we do to improve the information ?