Technical FAQs

Ask a Question

Does Schneider Electric have a solid state relay offer?

 Schneider Electric offers a range of solid state relays.

 The Schneider Electric SSR solid state relays have the following benefits over electromechanical relays;
  • Silent operation
  • Suitable for high frequency operation  (high operating rates)
  • Resistance to vibrations
  • Suitable for high number of operations (no moving parts to 'wear out'
 The SSR solid state relay offer from Schneider Electric are available in two mounting methods;
  • For panel mounting ('Hockey puck' style) type: SSRPxxxxx,
  • DIN rail mounting type; SSRDxxxxx.

 Each relay has 1 N/O contact, the main characteristics including input voltage, output voltage and current ranges are as outlined below for each of these styles;


Was this helpful?
What can we do to improve the information ?