Technical FAQs

Ask a Question

How can I assign the IP address to the TwidoPort 499TWD01100 gateway?

When the TwidoPort module is configured with TwidoSuite or TwidoSoft, its IP configuration is stored in the Twido PLC.

The IP configuration is therefore set in the Twido configuration and as a result, maintenance staff can replace TwidoPort modules with no need for any further configuration operations (carried out using the Plug and Play standard).
To use this Plug and Play function, you will need TwidoSuite or TwidoSoft V3.0 or later and a PLC OS V3.0 or later.
If you have an earlier version of TwidoSoft or if the TwidoPort operates in BootP, Telnet must be used to configure TwidoPort manually. 
Was this helpful?
What can we do to improve the information ?