Technical FAQs

Ask a Question

What is the part number for the neutral pole for a 50 A VCF3GE switch ?

For the 50 A VCF3GE switch, the neutral pole with early make and late break contacts (part number VZ12) is an add-on module. Caution: In the 08 online catalogue, this module is declared for a 63 A to 80 A rating, whereas in reality, it is a 50 A to 63 A rating (08 online catalogue error).
Was this helpful?
What can we do to improve the information ?