Technical FAQs

Ask a Question

What is the maximum distance supported for Connexium DRS switches TCSESM063F2CU1 and A TCSESM063F2CS1.

A TCSESM063F2CU1 ConneXium extended managed switch, which supports multi-mode fiber cable  and can achieve distances on the main ring up to 2 km.
A TCSESM063F2CS1 ConneXium extended managed switch, which supports single-mode fiber cable and can achieve distances on the main ring up to 15 km.
 
Was this helpful?
What can we do to improve the information ?