Technical FAQs

Ask a Question

Why in the Quantum 140CRA drop the ComAct led is not glowing

Basically when there is no IO card in a CRA drop the In & Out Bytes for that particular drop is zero (see enclosed pic), mean there is no data to exchange between CRP & CRA module; Hence in this case the CRA com act would be in off position. This is normal behaviour, and doesn't represent any fault. Any type of fault on a drop is represented by the FAULT led and ComAct led blinking sequence
Was this helpful?
What can we do to improve the information ?