Technical FAQs

Ask a Question

What to do if my UPS SURT15KUXI is showing "UPS Is Overloaded"?

Kindly check the following condition if the SURT15KUXI is overloaded: 

1) Decrease the load
2) Check the load distribution on the three phases through the Power View display. 
3) If the load is unevenly distributed, adjust the load distribution.
Was this helpful?
What can we do to improve the information ?