Technical FAQs

Ask a Question

How to clear Output off error in SRCE6KUXI model ?

Kindly follow the below instructions to solve the output off error in SREC6KUXI model:

• Input supply should be on to the UPS.

• Turn on the UPS [display should be on].

• Click on ‘Enter’ button for Main Menu.

• Select the ‘Control’ option from Main Menu and enter on it.

• Inside the ‘Control’ option, select second option ‘Output Control’ and click enter on it.

• Again enter on the option ‘No Action’ and it starts to flash for the changes.

• Enter down arrow button until you find the option ‘Turn on Output’.

• Click enter button on ‘Turn on Output’ option to turn on the output.

• Press Mute/Esc button twice to return to main screen.

• Recheck the output voltage from main screen it should be ‘230v’
Was this helpful?
What can we do to improve the information ?