Technical FAQs

Ask a Question

How to mute audiable alarm in SRC2KUXI ?

Follow the steps to configure parameters in the UPS:1. Press the ENTER button.
2. Press the UP/DOWN ARROW buttons to navigate to “Set”.
3. Press the ENTER button.
4. Navigate through the parameters using the UP/DOWN ARROW buttons.
5. Press the ENTER button to edit the Audible alert (3rd Option). Speaker Icons start flashing to indicate
the editing.
6. Press the UP/DOWN ARROW buttons to navigate between the options
available for the selected parameter(Enable or disable),Factory
Default setting will be Enable.
7. Press the ENTER button to select the option or MUTE/ESC button to abort
the editing of current parameter. Flashing of icons stops after this.
8. Press the UP/DOWN ARROW buttons to navigate between parameters.
9. Press the MUTE/ESC button to exit menu navigation.
Was this helpful?
What can we do to improve the information ?