Technical FAQs

Ask a Question

How to mute audiable alarm in SRC6KUXI ?

Follow the steps to configure parameters in the UPS:
1. Press the ENTER button.
2. Press the UP/DOWN ARROW buttons to navigate to configurations.
3. Press the ENTER button.
4. Using the UP/DOWN ARROW buttons select Configuration.
5. Press the ENTER button to select Configuration.
6. Navigate through the parameters using the UP/DOWN ARROW buttons and select Display setting.
7. Press the ENTER button to edit a Display setting. Icons start flashing to indicate
the editing.8. Navigate through the parameters using the UP/DOWN ARROW buttons and select Battery Beep Enable.
9. Press the ENTER button to edit a Battery Beep Enable. Icons start flashing to indicate
the editing.
10. Press the UP/DOWN ARROW buttons to navigate between the options
available Enable or Disable (factory default will be enabled).
11. Press the ENTER button to select the option or MUTE/ESC button to abort
the editing of current parameter. Flashing of icons stops after this.
12. Press the UP/DOWN ARROW buttons to navigate between parameters.
13. Press the MUTE/ESC button to exit menu navigation.
Was this helpful?
What can we do to improve the information ?