Technical FAQs

Ask a Question

What is the Output Frequency Options in Alarm SURT20KUXI ?

Output Frequency Options:

Auto Sensing; 50 Hz; 60 Hz
50 Hz frequency range: 50±3 Hz; 50±0.1 Hz
60 Hz frequency range: 60±3 Hz; 60±0.1 Hz
Was this helpful?
What can we do to improve the information ?