Technical FAQs

Ask a Question

Can we set the high and low voltage thersold to intervene the battery backup in PCPE

Yes, Open the application, click on Voltage' under the 'Confuguration' menu, select 'the maximum and the minimum voltage from the drop down list and click on apply to save the changes.
Was this helpful?
What can we do to improve the information ?