Technical FAQs

Ask a Question

While uninstalling PowerChute, a dialog says files are locked or read-only.

Close all PowerChute components like the user interface, and files such as the release notes. Then, click Yes or Retry on the dialog to proceed with the uninstallation. This ensures that all PowerChute files are removed during the uninstallation. 
Was this helpful?
What can we do to improve the information ?