Technical FAQs

Ask a Question

Which protocols can I use to communicate Micom Relays with Power Scada Expert.

To communicate Micom Relay with PSE, you have two ways to communicate :

1. Using Modbus Protocol, then you need to simply create an IO Device in PSE with Modbus/Modnet protocol (depends on the Micom relay model if that supports) and need to read the registers of the Micom Relay to get the RMS value etc like we did for the other energy meters.

2. Using IEC61850 protocol, then kindly follow the attached procedure to communicate PSE with Micom Relay over IEC61850 protocol. You need to confirm that your Micom Relay model supports this protocol or not.
 
Was this helpful?
What can we do to improve the information ?