Technical FAQs

Ask a Question

Which pressure switch model do we select to shut down the pump if the pressure is over 25 bar.

To operate a pump above 25 bar , you can refer our Electro Mechanical pressure switches like below :

1. XMLA035A2S12 (pressure switch XMLA 35 bar - fixed scale 1 threshold - 1 C/O)

2. XMLA035A2S11 (pressure switch XMLA 35 bar - fixed scale 1 threshold - 1 C/O)

3. XMLA035A2C11 (pressure switch XMLA 35 bar - fixed scale 1 threshold - 1 C/O)

 
Was this helpful?
What can we do to improve the information ?