Technical FAQs

Ask a Question

How can we create an Editable Drop Down List of String Tag in Vijeo Citect.

To use this drop downlist in Vijeo Citect SCADA with editable tags you need to use an ActiveX combo box:

Paste the activeX control “Microsoft Forms 2.0 ComboBox” on a graphics page

Associate the TEXT property with a Tag. This tag will contain the value of the item selected from the ComboBox.


FUNCTION MyPageLoad()
OBJECT oComboBox1
INT iIndex
oComboBox1 = ObjectByName("AN210")
_ObjectCallMethod(oComboBox1,"Clear")
_ObjectCallMethod(oComboBox1,"AddItem","Tag1",iIndex)
iIndex = iIndex + 1
_ObjectCallMethod(oComboBox1,"AddItem","Tag2",iIndex)
iIndex = iIndex + 1
_ObjectCallMethod(oComboBox1,"AddItem","Tag3",iIndex)
END

You need to call this function MyPageLoad() on your graphics page properties >> Events >> On Page Entry .
 
Was this helpful?
What can we do to improve the information ?