Technical FAQs

Ask a Question

How can I get an alarm if my only trend servers stops.

If only trend server stops then you can generate an alarm using the function
"ServerIsOnline("Trend Server Name", "Cluster Name") "

If the Trend Server is offline then it will give return value of 0 otherwise 1 if server is online.
 
Was this helpful?
What can we do to improve the information ?