Technical FAQs

Ask a Question

How to configure battery AH in UPS SRC10KUXI?

To set the battery Ah follow the below steps                                                
1. Press the ENTER button.
2. Press the UP/DOWN ARROW buttons to navigate to “SET”.
3. Press the ENTER button.
4. Navigate through the parameter using the UP/DOWN ARROW buttons.
5. Press the ENTER button to edit a parameter. Icons(BAT, Ah appears on left hand side) start flashing to indicate the editing
6. Press the UP/DOWN ARROW buttons to navigate between the options available for the selected parameter.
7. Press the ENTER button to select the option or MUTE/ESC button to abort the editing of current parameter. Flashing of icons stops after this.
8. Press the UP/DOWN ARROW buttons to navigate between parameters.
9. Press the MUTE/ESC button to exit menu navigation
Was this helpful?
What can we do to improve the information ?