Technical FAQs

Ask a Question

Is it possible to mount ZENL contact block in XALD03 enclosure.

Yes, it is possible.
The contact blocks ZENL are mounted on a metal mounting plate in the back of the XALD enclosure.
Was this helpful?
What can we do to improve the information ?