Technical FAQs

Ask a Question

How to switch Remote mode to Local mode on ATV303 drive.

=>Power on the Drive
=>display shows “- - 00”
=>pressed Mode button for 3 second
=>then display shows “- - 00” and only one LED is flashing and moving. Adjust the frequency with the wheel and press “RUN” to run the drive. It is Local Mode
=>then pressed ESC button for 2 second and then display shows “- - 00” and three LED is flashing. Still dive is in Local Mode, but it is not possible to  adjust the  frequency with the wheel. Need to press ENT to switch to REF menu.
=>again then pressed ESC button for 2 second then only one LED is flashing and moving.
=>then pressed Mode button for 3 second and display shows “- - 00” without any LED flashing. It is Remote Mode.
 
Was this helpful?
What can we do to improve the information ?