Technical FAQs

Ask a Question

Is ATV71 drive comply any standard for voltage dip.

ATV71 is complied with IEC61800-3, which contains the IEC61000-4-11 (Testing and measurement techniques – Voltage dips, short interruptions and voltage variation immunity tests).

 
Was this helpful?
What can we do to improve the information ?