Technical FAQs

Ask a Question

Is it possible to achieve holding torque on ATV71 drive.

If you install an encoder on the motor and feedback this to the ATV71encoder card,
Then at zero speed of ATV71 drive with run command, holding torque is achievable.
Was this helpful?
What can we do to improve the information ?