Technical FAQs

Ask a Question

What is the application of PRD-DC surge arrestors.

The PRD-DC surge arresters are the type 2 withdrawable surge arresters for photovoltaic applications.
PRD-DC direct current surge arresters are designed to protect against overvoltages due to a lightning strike: of the "DC" input to the inverter and of photovoltaic panels. It should be installed in a switchboard inside the building. If the switchboard is located outside, it must be weatherproof. Withdrawable PRD-DC surge arresters allow damaged cartridges to be replaced quickly. They offer remote reporting of the "cartridge must be changed" message.

Please refer below the catalog references of this offer.


 
Was this helpful?
What can we do to improve the information ?