Technical FAQs

Ask a Question

If the distance between the "generator" part and the "conversion" part, is more than 10m , is it required to use two surge arresters or more, to ensure protection of each of the two parts.

Yes, if the distance between the "generator" part and the "conversion" part, is more than 10m , it is required to use two surge arresters or more, to ensure protection of each of the two parts.



 
Was this helpful?
What can we do to improve the information ?