Technical FAQs

Ask a Question

What is the degree of protection (IP) of PRD-DC surge arresters.

The degree of protection (IP) as per IEC 60529 for PRD-DC surge arresters is 

*Device only >> IP20
*Device in modular enclosure >> IP40
 
Was this helpful?
What can we do to improve the information ?