Technical FAQs

Ask a Question

What is the operating and storage temperature of PRD-DC surge arrester.

The operating and storage temperature of PRD-DC surge arrester is 

*Operating temperature -25°C to +60°C
*Storage temperature -40°C to +85°C
Was this helpful?
What can we do to improve the information ?