Technical FAQs

Ask a Question

Whais the Tropicalization (IEC 60068-1) of PRD-DC surge arrester.

The Tropicalization (IEC 60068-1) of PRD-DC surge arrester is Treatment 2 (relative humidity of 95 % at 55°C).
Was this helpful?
What can we do to improve the information ?