Technical FAQs

Ask a Question

Is it possible to provide electrical interlock between NSX breaker using only IVE in changeover system.

It is possible to provide electrical interlock between NSX breaker using IVE 
and MCCBs installed on the interlock plate + IVE can be proposed in both voltages DC or AC, 
but it is necessary that voltage should be either DC or either AC for IVE+Motor mechanism.
Was this helpful?
What can we do to improve the information ?