Technical FAQs

Ask a Question

Does PowerLogic PM8000 allow us to daisy chain other PM8000 meters via Ethernet?

The PM8000 has the same dual Ethernet port function as the PM5500 series meters. So you can daisy-chain multiple PM8000 using the Ethernet connections.
Was this helpful?
What can we do to improve the information ?