Technical FAQs

Ask a Question

For how much time CPU backup will be retained if both power and battery is not available with TSXPSY2600.

The backup time depends on the ambient temperature. Assuming that the processor was switched on previously, the typical backup time varies in the following way.
 
Ambient temperature when switching off 20°C 30°C 40°C 50°C
Backup time 2h 45mn 20mn 8mn

Was this helpful?
What can we do to improve the information ?