Technical FAQs

Ask a Question

Will the breaker trip when ZSI testing is performed on NW Upstream and downstream Breaker using FFTK

Through the FFTK, ZSI test do not operate the breaker. Is a visual test on the micrologic display. No tripping occures.
The breaker can be in open or close position during the test, it doesn't matter.

Was this helpful?
What can we do to improve the information ?