Technical FAQs

Ask a Question

What is the maximum number of Modbus slaves which can be configured to Com'X 200

Maximum no of modbus slaves which can be configured to Com'X 200 is 20. 
Please refer attached file.
Was this helpful?
What can we do to improve the information ?