Technical FAQs

Ask a Question

What is the "Response time t(an)" for Insulation Monitoring Device Vigilohm IM10-H and IM20-H (Healthcare application).

Vigilohm IM10-H and IM20-H are compliant to IEC61557-8, Ed 2014, including § A.2.4.2   “Response time”;
Reference to the standard is as below;
Was this helpful?
What can we do to improve the information ?