Technical FAQs

Ask a Question

What is the maximum display measured value insulation resistance by Insulation Monitoring Device Vigilohm IM20-H (Healthcare application).

IM20-H, displays Insulation resistance up to 10 Mega Ohm.
Was this helpful?
What can we do to improve the information ?