Technical FAQs

Ask a Question

How many maximum option modules can be added to PowerLogic PM8000 series meter considering operating temperature specifications.

Upto 4 number of option modules can be attached to PowerLogic PM8000 series meter.
Maximum operation temperature is based on the quantity and type of attached option modules. Refer below specifications;
Was this helpful?
What can we do to improve the information ?