Technical FAQs

Ask a Question

What are the control power input requirements for PowerLogic PM8000 series meter?

Control power
• AC at 50/60 Hz ± 10%: 90 to 415 V ± 10%
• AC at 400 Hz: 90 to 120 V ± 10%
• DC: 120 to 300 V DC ± 10%
• Burden values for meter only
◦◦ AC burden at 45 to 65 Hz: max. 7.2 W / 18 VA at 415 V
◦◦ AC burden at 400 Hz: max. 4.5 W / 8 VA at 120 V
◦◦ DC burden: max. 6 W at 300 V DC
• Burden values for fully optioned meter
◦◦ AC burden at 45 to 65 Hz: max. 18 W / 36 VA at 415 V
◦◦ AC burden at 400 Hz: max. 18 W / 28 VA at 120 V
◦◦ DC burden: max. 17 W at 300 V DC
• Overvoltage category III
Was this helpful?
What can we do to improve the information ?