Technical FAQs

Ask a Question

What is the rating of the current inputs for PowerLogic PM8000 series meter?

Rating of current inputs;
  • Nominal 5 A (Class 0.2S) or 1 A (Class 0.5S)
  • Measured current: 50 mA to 10 A
  • Starting current: 5 mA
  • Withstand: 20 A continuous, 50 A @10 sec/hr, 500 @ 1 sec/hr
  • Impedance: 0.3 mOhm
  • Burden: 0.024 VA at 10 A
Was this helpful?
What can we do to improve the information ?