Technical FAQs

Ask a Question

What is PowerLogic PM8000 default IP address, username, and password ?

The default IP address is 

The username and password are defined by your meter’s security configuration; if standard security is enabled, the password is the same as the display password with a default username of 8000.
The default username is admin.
The default display password is 0.
Was this helpful?
What can we do to improve the information ?