Technical FAQs

Ask a Question

How to upgrade Com'X firmware using the USB port

1. Save the firmware file at the root of the USB memory key.

2. Rename the file to upgrade.sp1.

3. Make sure there is no file located at the root of the USB memory key with a name that is the same as the serial number of the Com'X 510.

4. Power down the Com'X.

5. Insert the USB memory key in the USB port located on the front face.

6. Power up the Com'X.

7. Wait for the Com'X to reboot. The power LED turns green when the reboot is complete.

8. Connect to the Com'X through a PC and click the About link to check that the new firmware is installed.
Was this helpful?
What can we do to improve the information ?