Technical FAQs

Ask a Question

Does the Acti 9 C60H-DC is UL listed.

There are 2 different C60H-DC global offers. 
- MGN615xx C60H-DC ("Multi9 grey material) for OEM applications (with IEC / UL / CCC now !) 
- A9N615xx C60H-DC (Acti9 white material) for standard applications (with IEC only) 
The white material is not compliant with OEM requirements & UL certification. 
Was this helpful?
What can we do to improve the information ?