Technical FAQs

Ask a Question

Which PM5000 series meter firmware versions available with QR codes and 32 bit energy register

The new firmware for PM5000 with QR codes and 32 bit energy register are now available on schneider-electric.com. The versions are different depending on the meter model, please check below:

PM5110, PM5310, PM5330: V01.03.07.38
PM5320, PM5340: V01.03.07.23
PM5560: V1.01
 
You will need the DLF tool to upgrade the firmware. Upgrade instructions are available on the user guide.
Was this helpful?
What can we do to improve the information ?