Technical FAQs

Ask a Question

Is is possible to use Auxiliary connector of MW2 Blokset at operation voltage of 415 V AC and what is the insulation voltage of these Auxiliary connectors.

Auxiliary Connectors of Blokset have Rated Operational Voltage (Ue) of 230V AC Maximum and Rated Insulation Voltage of 500V.

So it is not possible to use these connectors where a application requires these connectors to be used at 415V AC.

 
Was this helpful?
What can we do to improve the information ?