Technical FAQs

Ask a Question

Is Altivar Process drive fulfills the standard IEC60721-3-3 class 3C3.

Yes, Altivar Process drive is fulfills the standard IEC60721-3-3 class 3C3.
 
Was this helpful?
What can we do to improve the information ?