Technical FAQs

Ask a Question

What is the minimum power supply voltage without any fault for ATS48 Soft Starter.

The minimum power supply voltage without any fault is 200V. ATS48 will start the motor but with low torque.
If the torque is not high enough, the motor doesn't start and the ATS48 will trip in OHF or OLF.

 
Was this helpful?
What can we do to improve the information ?