Technical FAQs

Ask a Question

How can we set the Output Frequency using the display for SURT15KUXI ?

Kindly follow the below steps to set the frequency for SURT15KUXI using diplay:

1.Click on ‘Enter’ button for Main Menu.
2. Select the ‘Setup’ option from Main Menu and enter on it.
3. Inside the 'Setup'option, select third option ‘System’ and click enter on it.
4. Again enter on the option and select Frequency as per the below options:

Output Frequency Options:

Auto Sensing; 50 Hz; 60 Hz
50 Hz frequency range: 50±3 Hz; 50±0.1 Hz
60 Hz frequency range: 60±3 Hz; 60±0.1 Hz
Was this helpful?
What can we do to improve the information ?